Nexperia announces industry’s smallest logic parts approved for automotive
February 26, 2019Nijmegen -- Up to 64% smaller than leaded devices
Nexperia, the global leader in discretes, logic and MOSFET devices, today announced that over twenty logic types in the company’s space-saving leadless MicroPak packages are now AEC-Q100 qualified. These logic solutions are the smallest devices of their type suitable for automotive applications and Nexperia’s Q100 portfolio exceeds the Automotive Electronics Council’s requirements.
Nexperia’s MicroPak packages feature the same silicon die as larger PicoGate options, ensuring that electrical performance remains identical to leaded equivalents. MicroPak packages save up to 64% PCB space compared to leaded equivalents while providing a more reliable bond between device and board, thanks to a higher pad size-to-package footprint ratio.
Nexperia’s complete MicroPak range is very broad and includes gates, analog switches, buffers / inverters / drivers, bus switches, translators, flip-flops, decoders / demultiplexers, multiplexers, latches, level shifters and Schmitt-trigger devices.
Twenty solutions in XSON6 (SOT886 and SOT1202) and XSON8 (SOT833-1 and SOT1203) packages are available immediately in Nexperia’s Automotive portfolio – including low-power single-gate and dual-gate functions in AUP (0.8 V to 3.6 V), AVC (1.2 V to 3.6 V) and LVC (1.65 V to 5.5 V) technologies, ranging from gates to translators. In addition, more devices from Nexperia’s MicroPak offering can be released for automotive applications upon request.
Ghislaine Jilisen-Janssen, Product Manager for Mini Logic, commented: “These are the smallest logic parts qualified for the automotive industry. Applications include in-car entertainment and ADAS (Advanced Driver Assist Systems) where miniaturisation is of paramount importance.”
For more information visit https://www.nexperia.com/products/logic/family/MICROPAK/ or download the MicroPak logic brochure.
About Nexperia
Nexperia, the former Standard Products division of NXP, is a dedicated global leader in Discretes, Logic and MOSFET devices. The company became independent at the beginning of 2017. Focused on efficiency, Nexperia produces consistently reliable semiconductor components at high volume: More than 90 billion annually. Our extensive portfolio meets the stringent standards set by the Automotive industry. Industry-leading, miniature packages, produced in our own manufacturing facilities, combine power and thermal efficiency with best-in-class quality levels.
With over 50 years history supplying to the world’s biggest companies, Nexperia has over 11,000 employees across Asia, Europe and the U.S., offering global support. The company has an extensive IP portfolio and is certified to ISO9001, ISO/TS16949, ISO14001 and OHSAS18001.
Nexperia: Efficiency wins.
For press information, please contact:
| Nexperia | Agency: BWW Communications |
|
Petra Beekmans, Head of Communications & Branding |
Nick Foot, director |