Press releases
Energy harvesting PMIC from Nexperia enables ...
Capacitive DC-DC converter enables up to 90% BOM cost savings.
Read moreNexperia introduces the first application-specific ...
Additional 40% lower RDS(on) and increase power density by 58x for telecom & computing hot-swap ...
Read moreNexperia introduces in-vehicle network ESD ...
A variety of packages, capacitance classes and 36 V VRWM provide design flexibility for ...
Read moreNexperia’s response to news that semiconductors are ...
Nexperia strongly condemns the illegal invasion of Ukraine by Russia. We comply with ...
Read moreNexperia announces two new additions to their TrEOS ...
Combining high surge robustness with very low trigger and extremely low clamping voltages, the ...
Read moreNexperia releases ultrafast 650 V Recovery ...
Latest additions to a growing portfolio of CFP power diodes
Read moreNexperia launches new hotswap Application Specific ...
Fully optimised RDS(on) & SOA manage in-rush currents in 12 V hotswap and soft start applications
Read moreNexperia is shocked by the Secretary of State’s ...
UK Government’s decision creates further uncertainty for Nexperia employees in Wales
Read moreNexperia invests in sustainable alternatives to ...
Investment boosts existing power management expertise
Read moreNexperia to demonstrate full range of automotive ...
For the first time Nexperia will be part of electronica with a presence in Hall C3, booth 319.
Read more