Nexperia’s transformer drivers improve efficiency and performance in industrial and automotive applications
September 19, 2024Nijmegen -- Push-pull drivers enable 6 W of power delivery at up to 90% efficiency in a small, SOT package
Nexperia introduced the NXF6501-Q100, NXF6505A-Q100, and NXF6505B-Q100 today. These are AEC-Q100 qualified, push-pull transformer drivers that enable the design of small, low-noise and low-EMI isolated power supplies for a range of automotive applications like traction inverters and motor control, DC-DC converters, battery management systems and on-board chargers in electric vehicles (EV). These transformer drivers are also suitable for use in industrial applications like telecommunications, medical applications, instrumentation and industrial automation equipment, solar inverters, energy meters, and programmable logic controllers (PLC).
The NXF650x(A/B)-Q100 series can drive low-profile, center-tapped transformers from a 2.25 V to 5.5 V power supply with high output current (1.2 A at 5 V) and high efficiency (up to 90%). To enable small form factor designs, the devices have a 440 kHz (NXF6501 and NXF6505B) or 160 kHz (NXF6505A) internal oscillator and a gate drive circuit that produces complementary output signals to drive internal ground-referenced n-channel power switches. Alternatively, a clock signal can be applied externally to the NXF6505A and NXF6505B to enable precise control of switching harmonics or enable synchronization of multiple NFX6505x(A/B) -Q100 devices. Additionally, the NXF650x(A/B)-Q100 series employs slew rate control and spread-spectrum clocking (SSC) to deliver ultra-low noise and electromagnetic interference (EMI).
The NXF650x(A/B)-Q100 series also includes a comprehensive range of internal protection features such as over-current protection (1.7 A) with hiccup mode, under-voltage lockout, thermal shutdown, and break-before-make circuitry to ensure safe operation. Additionally, these transformer drivers have a soft-start (~5 ms) feature that prevents high inrush currents during power-up with large load capacitors. Lastly, these devices have fail-safe inputs that prevent back-powering of the local power supply and eliminate the need for power sequence management.
These devices are available in compact industry-standard footprints like the 5-pin SOT8098 (TSOT5) and 6-pin SOT8061 (TSOT6) package and safely operate in ambient temperatures ranging between -55 °C and 125 °C. To learn more about Nexperia’s portfolio of transformer drivers visit https://www.nexperia.com/products/analog-logic-ics/isolation/transformer-drivers
About Nexperia
Headquartered in the Netherlands, Nexperia is a global semiconductor company with a rich European history and over 14,000 employees across Europe, Asia, and the United States. As a leading expert in the development and production of essential semiconductors, Nexperia’s components enable the basic functionality of virtually every commercial electronic design in the world – from automotive and industrial to mobile and consumer applications.
The company serves a global customer base, shipping more than 100 billion products annually. These products are recognized as benchmarks in efficiency – in process, size, power, and performance. Nexperia's commitment to innovation, efficiency, sustainability, and stringent industry requirements is evident in its extensive IP portfolio, its expanding product range, and its certification to IATF 16949, ISO 9001, ISO 14001 and ISO 45001 standards.
For press information, please contact:
Nexperia
Anne Proch
Tel: +49 160 916 884 18
Email: anne.proch@nexperia.com
Publitek
Megan King
Tel: +44 7855060775
E-mail: megan.king@publitek.com