Pioneering interactive datasheets from Nexperia put MOSFET behavior analysis at engineers’ fingertips
May 10, 2023Nijmegen -- Removing manual calculation, parameters dynamically respond to user inputs
![](/.imaging/mte/nexperia/page-intro/dam/nexperia/About-new_final/News-and-Events/Press-release/press-releases/Pioneering-interactive-datasheets-from-Nexperia-put-MOSFET-behavior-analysis-at-engineers--fingertips/2023-0001-NEX_064_PR-image---interactive-datasheets_V03.jpg/jcr:content/2023-0001%20NEX_064_PR-image%20-%20interactive%20datasheets_V03.jpg)
Nexperia, the essential semiconductor expert, today announced a significant raising of the bar in semiconductor engineer design support with the release of next-generation interactive datasheets to accompany its Power MOSFETs. By manipulating interactive sliders within the datasheets, users can manually adjust the voltage, current, temperature and other conditions for their circuit application and watch how the operating point of a device dynamically responds to these changes.
These interactive datasheets effectively offer a type of graphical user interface to a circuit simulator, using Nexperia’s advanced electrothermal models to calculate the operating point of a device. In addition, they allow engineers to visualize immediately the interaction between parameters such as gate voltage, drain current, RDS(on) and temperature. Their collective contribution to the device behavior is then displayed dynamically in tables or graphs. As a result, Nexperia’s interactive datasheets can significantly increase productivity by eliminating the time needed for an engineer to perform manual calculations or set up and debug a circuit simulation.
The datasheet is commonly the first port of call when a design engineer is looking to select a device for an application. However, while they contain a wealth of information, including the minimum, maximum and typical specifications across dozens of device parameters, it is often difficult to determine how these are interrelated. Consequently, engineers must perform time-consuming manual calculations or set up a circuit simulator using models provided by the manufacturer (assuming these are available) to thoroughly investigate a device’s behavior. Even then, many manufacturers’ simulation models do not show the effect of temperature changes on device behavior. The new interactive datasheets from Nexperia support engineers by showing real-time interaction across different parameters as they are manually changed with the easy-to-use datasheet sliders.
Chris Boyce, Senior Director of Nexperia’s Power MOSFET business adds, “Whether you are a Design Engineer looking to see how a device will perform at elevated temperature, or a Component Engineer trying to compare devices under different test conditions, our new interactive datasheets are designed to make your life easier.”
The technology powering these datasheets is the same as that used in Nexperia’s hugely successful precision electrothermal MOSFET models, which demonstrate how the behaviour of discrete MOSFETs changes with temperature. The new interactive datasheets are offered in addition to the traditional static datasheets and operate in any standard web browser without the requirement of additional software for device simulation.
With the initial version currently under patent application, Nexperia will be reaching out to its global community of customer engineers to evaluate how interactive datasheets are used in real-time in order to broaden the functionality of future versions.
More than 200 interactive datasheets are already available, covering the devices in Nexperia’s latest generations of Automotive and Industrial Power MOSFETs. Over time, the Company plans to make them available for its entire portfolio of discrete MOSFETs and other devices.
Try a live interactive datasheet in action at nexperia.com/interactive-datasheet
About Nexperia
Headquartered in the Netherlands, Nexperia is a global semiconductor company with a rich European history and over 15,000 employees across Europe, Asia, and the United States. As a leading expert in the development and production of essential semiconductors, Nexperia’s components enable the basic functionality of virtually every electronic design in the world – from automotive and industrial to mobile and consumer applications.
The company serves a global customer base, shipping more than 100 billion products annually. These products are recognized as benchmarks in efficiency – in process, size, power, and performance. Nexperia's commitment to innovation, efficiency, sustainability, and stringent industry requirements are evident in its extensive IP portfolio, its expanding product range and its certification to IATF 16949, ISO 9001, ISO 14001 and ISO 45001 standards.
For press information, please contact:
Nexperia
Judith Schröter
Phone: +49 170 8586403
Email: judith.schroeter@nexperia.com
Publitek
Megan King
Tel: +44 7855060775
E-mail: megan.king@publitek.com