New Trench Schottky rectifiers from Nexperia increase efficiency for fast switching applications
May 04, 2021Nijmegen -- AEC-Q101 approved devices up to 100 V and 20 A combine low switching losses and increased safe operating area
![](/.imaging/mte/nexperia/page-intro/dam/nexperia/About-new_final/News-and-Events/Press-release/press-releases/New-Trench-Schottky-rectifiers-from-Nexperia-increase-efficiency-for-fast-switching-applications/Nexperia_Press-image_Trench-Schottky-rectifiers.jpg/jcr:content/Nexperia_Press%20image_Trench%20Schottky%20rectifiers.jpg)
Nexperia, the expert in essential semiconductors, today extended its portfolio of Trench Schottky rectifiers with devices rated at up to 100 V and 20 A. The new parts feature excellent switching behavior and leading thermal performance. They are available in Nexperia’s Clip Bond FlatPower (CFP) packages which have a much smaller footprint than SMA/SMB/SMC components.
Trench technology results in low leakage and also greatly reduces the charge, Qrr, stored in the device. Therefore, Trench Schottky rectifiers deliver very fast switching, cutting both the switching losses of the rectifier and the losses that are induced in the MOSFET in the same commutation cell – a configuration that is commonly used in asynchronous switch-mode power converters. Nexperia’s PMEGxxxTx devices additionally provide a wide safe operating area (SOA), delivering an extra safety margin and reducing the risk of thermal runaway compared to parts currently available.
Jan Fischer, Nexperia’s product manager comments: “Nexperia’s Trench Schottky rectifiers combine low forward voltage and very low Qrr to enable best efficiency at high switching speeds as needed in switch-mode power converters. Automotive applications including LED lighting, in particular, will benefit from the wide SOA of our parts.”
Nexperia is investing in its portfolio of Trench Schottky rectifiers, now offering 32 devices from 40 V to 100 V and up to 15 A in volume production. A further 17 parts, including the 20 A types, are sampling. The PMEGxxxTx devices are housed in Clip Bond FlatPower packages CFP3/5/15(B). These size- and thermally-efficient packages have become the industry standard for power diodes. By featuring a solid copper clip, the packages’ thermal resistance is reduced and transfer of heat into the ambient environment is optimized, allowing small and compact PCB designs.
More details including datasheets are available at www.nexperia.com/trench-schottky-rectifiers. Designers can learn more about Nexperia’s Trench Schottky rectifiers by visiting Nexperia’s virtual booth at PCIM Digital Days 3-7 May at https://pcim.mesago.com. On Thursday 6th May, the company will present a free live webinar on this subject, entitled ‘Trench Schottky Rectifiers: How to increase the efficiency of your switch-mode power converter.’
About Nexperia
Nexperia is a leading expert in the high-volume production of essential semiconductors, components that are required by every electronic design in the world. The company’s extensive portfolio includes diodes, bipolar transistors, ESD protection devices, MOSFETs, GaN FETs and analog & logic ICs. Headquartered in Nijmegen, the Netherlands, Nexperia annually ships more than 90 billion products, meeting the stringent standards set by the automotive industry. These products are recognized as benchmarks in efficiency – in process, size, power and performance — with industry-leading small packages that save valuable energy and space.
With decades of experience in supplying to the world’s leading companies, Nexperia has over 12,000 employees across Asia, Europe and the US. Nexperia, a subsidiary of Wingtech Technology Co., Ltd. (600745.SS), has an extensive IP portfolio and is certified to IATF 16949, ISO 9001, ISO 14001 and OHSAS 18001.
Nexperia: Efficiency wins
For press information, please contact:
Nexperia | Agency: BWW Communications |
Petra Beekmans, Head of Communications & Branding |
Nick Foot, director |