Nexperia announces two new additions to their TrEOS family of ESD protection devices for high-speed data lines
December 14, 2022Nijmegen -- Combining high surge robustness with very low trigger and extremely low clamping voltages, the PESD4V0Y1BBSF and PESD4V0X2UM offer a highly effective solution for the protection of sensitive systems

Nexperia, the expert in essential semiconductors, has announced the latest additions to the Nexperia TrEOS portfolio, the PESD4V0Y1BBSF and PESD4V0X2UM extremely low clamping ESD protection diodes. These devices combine high surge robustness with very low trigger and clamping voltages and wide pass-bands, providing exceptional levels of immunity to surges, as demonstrated by their excellent IEC61000-4-5 ratings.
“Nexperia developed the TrEOS portfolio specifically to offer our customers a range of high-performance ESD protection solutions for applications such as USB3.2, USB4™, Thunderbolt™, HDMI 2.1 and Universal Flash,” said Stefan Seider, Senior Product Manager at Nexperia. “The fast-switching speeds of the PESD4V0Y1BBSF and PESD4V0X2UM deliver an extremely effective ESD peak suppression performance for high-speed while their low trigger voltage helps to reduce the energy content of IEC61000-4-5 8/20 µs surge pulses significantly.”
Available in the low-inductance DSN0603-2 package, the one-line PESD4V0Y1BBSF offers a trigger voltage of 6.3 V TLP combined with a typical device robustness and capacitance of 25 A 8/20 µs and 0.7 pF, respectively. The PESD4V0Y1BBSF offers a clamping voltage at 16 A 100 ns TLP of only 2.4 V, at 20 A 8/20 µs surge only 3.4 V. The two-line PESD4V0X2UM comes in the compact DFN1006-3 package and offers a trigger voltage of 8 V, combined with a typical device robustness exceeding 14 A 8/20 µs with a typical device capacitance of 0.82 pF.
While both devices offer excellent protection for USB2.0 D+/D- lines, the PESD4V0Y1BBSF has a S21 pass-band exceeding 7.5 GHz, making it suitable for USB3.x @ 5 Gbps. Both devices provide high levels of immunity to surges, as demonstrated by their excellent IEC61000-4-5 ratings.
For more information about these new parts, including product specifications and datasheets, visit nexperia.com/PESD4V0Y1BBSF and nexperia.com/PESD4V0X2UM. Nexperia’s complete Nexperia TrEOS portfolio is featured at nexperia.com/TrEOS
About Nexperia
Nexperia is a leading expert in the high-volume production of essential semiconductors, components that are required by every electronic design in the world. The company’s extensive portfolio includes diodes, bipolar transistors, ESD protection devices, MOSFETs, GaN FETs and analog & logic ICs. Headquartered in Nijmegen, the Netherlands, Nexperia annually ships more than 100 billion products, meeting the stringent standards set by the automotive industry. These products are recognized as benchmarks in efficiency – in process, size, power, and performance — with industry-leading small packages that save valuable energy and space.
With decades of experience in supplying to the world’s leading companies, Nexperia has over 14,000 employees across Asia, Europe, and the US. Nexperia, a subsidiary of Wingtech Technology Co., Ltd. (600745.SS), has an extensive IP portfolio and is certified to IATF 16949, ISO 9001, ISO 14001, and ISO 45001.
For press information, please contact:
Nexperia
Petra Beekmans, Head of Communications & Branding
Phone: +31 6 137 111 41
Email: petra.beekmans@nexperia.com
Judith Schröter
Phone: +49 170 8586403
Email: judith.schroeter@nexperia.com
Publitek
Björn Oberhössel
Phone: +49 4181 968098-30