Nexperia enhances Zener diode portfolio to address overswing and noise phenomena

Nexperia enhances Zener diode portfolio to address overswing and noise phenomena

September 12, 2024

Nijmegen -- 50 μA and general-purpose devices offer package flexibility for automotive and non-automotive applications

Nexperia today announced two enhancements to its extensive Zener diode portfolio that both eliminate undesirable overswing and noise behavior – making a major advancement in Zener technology. Firstly, the new 50 µA-Zener series with B-selection (Vz +/-2%)  and Vz ranging from 1.8 V to 51 V is offered in standard and automotive qualified variants. Making them ideal for automotive applications like on-board chargers in electric vehicles (EV) as well as for a broad range of industrial and consumer applications like general-purpose computing units, battery management systems, device chargers and smartwatches.

Nexperia’s new series of 50 µA devices now deliver full Zener functionality even at high voltages (up to 75 V). They have been designed to entirely eliminate the noise and overswing phenomena, common features of many Zener diodes that have previously led to application failures. These devices are available in small footprint packages including SOT23, SOD323, SOD523, and SOD123F as well as DFN1006BD-2 and DFN1006-2 with or without side-wettable flanks (SWF). The inclusion of SWF offers significant advantages, including highly reliable automated optical inspection (AOI) of solder joint quality and increased robustness of solder joints, enhancing the bond to the PCB compared to devices without SWF.

 

Furthermore, Nexperia also addresses overswing and noise concerns in their existing family of general-purpose PZU Zeners. This will provide engineers with greater flexibility for applications like supply voltage stabilization, comparison of sensor or supply voltages in addition to providing gate and avalanche breakdown protection for MOSFETs. The PZU family is available in SOD323, SOD323F, SOT23, DFN1006BD-2 and DFN1006-2 (2.4 V-51 V) packages, in both automotive and standard versions. Offering designers a viable alternative for critical applications that demand a sharper Zener ‘knee’, or where standard Zeners may show noise and overswing behavior.

 

Visit https://www.nexperia.com/zener to access product datasheets and learn more about Nexperia’s Zener diodes, including details on how the undesired overswing phenomena was eliminated.

About Nexperia

Headquartered in the Netherlands, Nexperia is a global semiconductor company with a rich European history and over 14,000 employees across Europe, Asia, and the United States. As a leading expert in the development and production of essential semiconductors, Nexperia’s components enable the basic functionality of virtually every commercial electronic design in the world – from automotive and industrial to mobile and consumer applications.


The company serves a global customer base, shipping more than 100 billion products annually. These products are recognized as benchmarks in efficiency – in process, size, power, and performance. Nexperia's commitment to innovation, efficiency, sustainability, and stringent industry requirements is evident in its extensive IP portfolio, its expanding product range, and its certification to IATF 16949, ISO 9001, ISO 14001 and ISO 45001 standards.

 

For press information, please contact:

Nexperia

Anne Proch

Tel: +49 160 916 884 18

Email: anne.proch@nexperia.com

 

Publitek

Megan King

Tel: +44 7855060775

E-mail: megan.king@publitek.com