Nexperia now offers GaN FETs in compact SMD packaging CCPAK for industrial and renewable energy applications
December 11, 2023Nijmegen -- Combining the benefits of copper-clip packaging and wide bandgap semiconductors
![](/.imaging/mte/nexperia/page-intro/dam/nexperia/About-new_final/News-and-Events/Press-release/press-releases/Nexperia-now-offers-GaN-FETs-in-compact-SMD-packaging-CCPAK-for-industrial-and-renewable-energy-applications/NEXP065_PR-Image-CCPAK.jpg/jcr:content/NEXP065_PR%20Image%20CCPAK.jpg)
Nexperia today announced that its GaN FET devices, featuring next-gen high-voltage GaN HEMT technology in proprietary copper-clip CCPAK surface mount packaging, are now available to designers of industrial and renewable energy applications. Building on two decades of expertise in supplying high-volume, high-quality copper-clip SMD packaging, Nexperia is now proud to extend its revolutionary packaging approach to GaN cascode switches in CCPAK. The GAN039-650NTB, a 33 mΩ (typ.) Gallium Nitride (GaN) FET within the CCPAK1212i top-side cooling package, ushers in a new era of wide bandgap semiconductors and copper-clip packaging. This technology offers advantages for renewable energy applications such as solar and residential heat pumps, further enhancing Nexperia’s commitment to developing the latest component technology for sustainable applications. It is also suited to a wide spectrum of industrial applications such as servo drives, switched-mode power supplies (SMPS), server, and telecom.
Nexperia’s CCPAK surface mount packaging uses Nexperia’s proven innovative copper-clip package technology to replace internal bond wires. This reduces parasitic losses, optimizes electrical and thermal performance, and improves device reliability. For maximum flexibility in designs, these CCPAK GaN FETs are available in top- or bottom-cooled configurations to further improve heat dissipation.
The cascode configuration of the GAN039-650NTB enables it to deliver superior switching and on-state performance, with a robust gate offering high margins against noise. This feature also simplifies application designs by eliminating the requirement for complex gate drivers and control circuitry, instead allowing them to be conveniently driven using standard silicon MOSFET drivers. Nexperia’s GaN technology improves switching stability and helps to shrink die size by approximately 24%. In addition, device RDS(on) is reduced to only 33 mΩ (typ.) at 25°C, with a high threshold voltage and low diode forward voltage.
“Nexperia recognizes that designers of industrial and renewable energy equipment need a highly robust switching solution that can provide excellent thermal efficiency when performing power conversion.”, according to Carlos Castro, Vice President and General Manager of the GaN FET business at Nexperia. “This is why Nexperia decided to bring together the exceptional switching performance of its cascode GaN FETs with the exceptional thermal properties of its CCPAK packaging to offer customers a compelling solution.”
Nexperia begins its CCPAK portfolio release with the top-cooled 33 mΩ (typ.), 650 V GAN039-650NTB, and will follow shortly with the bottom-cooled variant, GAN039-650NBB of the same RDS(on). More information including datasheets and samples is available at www.nexperia.com/ccpak.
About Nexperia
Headquartered in the Netherlands, Nexperia is a global semiconductor company with a rich European history and over 15,000 employees across Europe, Asia, and the United States. As a leading expert in the development and production of essential semiconductors, Nexperia’s components enable the basic functionality of virtually every commercial electronic design in the world – from automotive and industrial to mobile and consumer applications.
The company serves a global customer base, shipping more than 100 billion products annually. These products are recognized as benchmarks in efficiency – in process, size, power, and performance. Nexperia's commitment to innovation, efficiency, sustainability, and stringent industry requirements is evident in its extensive IP portfolio, its expanding product range, and its certification to IATF 16949, ISO 9001, ISO 14001 and ISO 45001 standards.
For press information, please contact:
Nexperia
Anne Proch
Tel: +49 160 916 884 18
Email: anne.proch@nexperia.com
Publitek
Megan King
Tel: +44 7855060775
E-mail: megan.king@publitek.com
Read in: Korean