Nexperia’s new step-down DC-DC converters with lowest quiescent current enhance design flexibility
January 21, 2025Nijmegen --
High efficiency converters deliver low output ripple from wide input voltage range
Nexperia today introduced a new series of step-down DC-DC converters featuring devices with outstanding stand-by and operating efficiency that offer engineers even greater flexibility for designing various fixed and portable battery-powered applications across consumer, industrial and automotive end-markets.
The NEX30606 is a high-efficiency, high-accuracy step-down converter that offers a choice of 16 resistor-settable output voltages from input voltages ranging from 1.8 V to 5.0 V. It can deliver up to 600 mA of output current and offers the industry’s lowest operating quiescent current (Iq) of 220 μA. This feature makes it ideal for wearable consumer applications like hearing aids, medical sensors, patches and monitors in addition to battery-powered industrial applications like smart meters, asset-tracking and industrial (IIOT) and narrow-band internet-of-things (NBIOT) devices. This device provides >90% switching efficiency for load currents ranging from 1 mA to 400 mA and has only 10 mV of output voltage ripple when stepping down from 3.6 V Vin to 1.8 Vout.
The NEX40400 step-down converter combines high efficiency (up to 8 % higher efficiency than close competition at low - mid load condition) with low operating quiescent current (60 μA typ.) and can provide up to 600 mA output from a wide 4.5 V to 40 V input range for applications. Featuring PFM (Pulse Frequency Modulation) for high efficiency at low to mid loads and Spread Spectrum Technology for minimizing EMI, the converter is ideal for industrial distributed power systems and grid infrastructure (e.g. smart e-meters) as well as consumer white goods. Low shutdown supply current (0.3 μA) also makes this converter suitable for use in battery-powered home appliances. Nexperia also plans to release an AEC-Q100 qualified version of the NEX40400 later in 2025 for use in automotive applications such as body electronics and lighting, in-vehicle infotainment (IVI) systems, advanced driver assistance systems (ADAS), as well as instrument clusters, cameras and displays.
Both the NEX30606 and NEX40400 offer traditional IC protection features such as Overcurrent Protection (OCP), short circuit protection, and thermal shutdown, ensuring reliability in demanding environments.
“Nexperia recognized the demand for high-efficiency, wide input-voltage range step-down DC-DC converters with low quiescent current that can serve multiple end-markets,” according to Irene Deng, General Manager of the IC Solutions business group at Nexperia. ”Devices in this new series offer industry-leading Iq and now provide engineers with even greater design flexibility across various industrial, consumer, and automotive applications.”
The NEX30606 is available in a space-saving WLCSP package measuring only 1.09 mm x 0.74 mm with a 0.35-mm pitch, which is almost 50% smaller than similar competing converters. The NEX40400 comes in a cost-effective 6-lead SOT8061-1 (TSOT23-6) plastic, surface-mounted package measuring 2.9 mm x 2.8 mm.
To learn more about Nexperia’s step-down DC-DC converters, visit: www.nexperia.com/dcdcconverter
About Nexperia
Headquartered in the Netherlands, Nexperia is a global semiconductor company with a rich European history and over 14,000 employees across Europe, Asia, and the United States. As a leading expert in the development and production of essential semiconductors, Nexperia’s components enable the basic functionality of virtually every commercial electronic design in the world – from automotive and industrial to mobile and consumer applications.
The company serves a global customer base, shipping more than 100 billion products annually. These products are recognized as benchmarks in efficiency – in process, size, power, and performance. Nexperia's commitment to innovation, efficiency, sustainability, and stringent industry requirements is evident in its extensive IP portfolio, its expanding product range, and its certification to IATF 16949, ISO 9001, ISO 14001 and ISO 45001 standards.
For press information, please contact:
Nexperia
Anne Proch
Tel: +49 160 916 884 18
Email: anne.proch@nexperia.com
Publitek
Lucy Sorton
Tel: +44 07966 301949
E-mail: lucy.sorton@publitek.com