Nexperia’s new bipolar junction transistors in DPAK-package deliver high reliability performance for automotive and industrial applications
July 29, 2021Nijmegen -- MJD series now available covering 2 – 8 A and 45 – 100 V and strengthening Nexperia’s power portfolio
![](/.imaging/mte/nexperia/page-intro/dam/nexperia/About-new_final/News-and-Events/Press-release/press-releases/Nexperia-s-new-bipolar-junction-transistors-in-DPAK-package-deliver-high-reliability-performance-for-automotive-and-industrial-applications/Nexperia_Press-image-DPAK-Package_MJD.jpg/jcr:content/Nexperia_Press-image-DPAK-Package_MJD.jpg)
Nexperia, the expert in essential semiconductors, today announced nine new power bipolar transistors, extending its portfolio of products in the thermally and electrically advantageous DPAK package to cover applications from 2 A to 8 A and from 45 V up to 100 V. The new MJD series parts are pin-to-pin compatible with other MJD devices in DPAK-package, and they also offer significant reliability benefits.
Available as automotive-qualified AEC-Q101 devices and industrial grade parts, the new MJD series bipolar transistors are rated at 2 A 50 V (MJD2873/-Q), 3 A 100 V (MJD31CH-Q), 4 A 45 V (MJD148/-Q), and 6 A 100 V (MJD41C /-Q and MJD42C /-Q). The MJD31CH-Q is designed as high gain version. All parts offer class-leading DPAK package reliability performance, with an industry-standard footprint. The bipolar transistors suit a wide range of applications such as LED automotive lighting; backlight dimming in LCD displays; linear voltage regulators; relay replacement; motor drives and MOSFET drivers.
Pedram Zoroofchi, Product Manager at Nexperia comments: “Nexperia is known as a high volume, high quality supplier for a broad customer base. By widening our MJD series of power bipolar transistors we provide designers with additional voltage-current options in a robust DPAK package. Therefore, our customers can benefit from the renowned quality and performance offered by Nexperia as a high-performance supplier.”
For more information, including product specs and datasheets, visit: www.nexperia.com/products/MJD
You can also view this new technology in action at Nexperia’s Power Live Event 21 – 23 September https://www.nexperia.com/power-live
About Nexperia
Nexperia is a leading expert in the high-volume production of essential semiconductors, components that are required by every electronic design in the world. The company’s extensive portfolio includes diodes, bipolar transistors, ESD protection devices, MOSFETs, GaN FETs and analog & logic ICs. Headquartered in Nijmegen, the Netherlands, Nexperia annually ships more than 90 billion products, meeting the stringent standards set by the automotive industry. These products are recognized as benchmarks in efficiency – in process, size, power and performance — with industry-leading small packages that save valuable energy and space.
With decades of experience in supplying to the world’s leading companies, Nexperia has over 12,000 employees across Asia, Europe and the US. Nexperia, a subsidiary of Wingtech Technology Co., Ltd. (600745.SS), has an extensive IP portfolio and is certified to IATF 16949, ISO 9001, ISO 14001 and OHSAS 18001.
Nexperia: Efficiency wins.
For press information, please contact:
Nexperia | Agency: BWW Communications |
Petra Beekmans, Head of Communications & Branding |
Nick Foot, director |