Next-generation fixed-direction voltage level translators from Nexperia reduce power consumption and pin count
December 10, 2024Nijmegen -- Solutions for applications with direction-controlled and auto-direction requirements

Nexperia today released a new family of next-generation fixed-direction voltage level translators ideal for use with some of the most commonly used push-pull data interfaces (including UART, SPI and JTAG protocols) as well as for general purpose input/output (GPIO). The NXU series of 4-bit, 2-bit, and 1-bit dual-supply buffers offer a smaller, higher performance and lower-cost level translation solution that simplifies communication between a host processor and peripheral I/O devices compared to existing designs in a broad range of consumer, industrial, automotive and enterprise applications.
Existing direction-controlled level translators typically require an additional GPIO pin for direction control, a requirement which increases device size while also adding to design complexity because it consumes I/O resources of the host processor. On the other hand, while auto-direction devices do not require a GPIO pin for direction control, they typically cannot provide the level of current drive required by many applications. Furthermore, they can sometimes exhibit non-deterministic I/O behavior resulting from one-shot architectures that can be time-consuming to debug. Another shortcoming of direction-controlled and auto-direction devices is that they typically consume too much power for power sensitive implementations.
Devices in Nexperia’s NXU family have been designed to combine the parametric performance capabilities of direction-controlled translation devices (i.e., high data rate, high drive strength, and glitch free power sequencing) with the lower pin-out and size advantages of auto-direction devices. The NXU translator devices consume significantly less power (>2x reduction) compared to auto-direction devices (for comparable bit counts). They also have a wider supply voltage range (0.9 V to 5.5 V) making the devices suitable for translating between any of the voltage nodes from 0.9 V up to 5 V. The NXU devices also support faster data rates (up to 250 Mbps) than other voltage translation solutions.
The NXU family of translators complements Nexperia’s existing portfolios of direction-controlled and auto-direction families of level translation devices by providing level translation solutions for applications that require a combination of auto-direction and direction-controlled capabilities. For maximum flexibility, various data-direction and package configurations are provided, while automotive-qualified (AEC-Q100) variants are also available in packages with side-wettable flanks to enable automated optical inspection.
To learn more about Nexperia’s voltage translation solutions visit:
www.nexperia.com/voltage_translators
About Nexperia
Headquartered in the Netherlands, Nexperia is a global semiconductor company with a rich European history and over 14,000 employees across Europe, Asia, and the United States. As a leading expert in the development and production of essential semiconductors, Nexperia’s components enable the basic functionality of virtually every commercial electronic design in the world – from automotive and industrial to mobile and consumer applications.
The company serves a global customer base, shipping more than 100 billion products annually. These products are recognized as benchmarks in efficiency – in process, size, power, and performance. Nexperia's commitment to innovation, efficiency, sustainability, and stringent industry requirements is evident in its extensive IP portfolio, its expanding product range, and its certification to IATF 16949, ISO 9001, ISO 14001 and ISO 45001 standards.
For press information, please contact:
Nexperia
Anne Proch
Tel: +49 160 916 884 18
Email: anne.proch@nexperia.com
Publitek
Lucy Sorton
Tel: +44 07966 301949
E-mail: lucy.sorton@publitek.com