New automotive TrEOS ESD protection from Nexperia combines high signal integrity, low clamping voltage and high surge robustness
September 15, 2020Nijmegen -- Industry-benchmark performance devices now AEC-Q101 qualified - protecting infotainment, multimedia and ADAS systems.
![](/.imaging/mte/nexperia/page-intro/dam/nexperia/About-new_final/News-and-Events/Press-release/press-releases/New-automotive-TrEOS-ESD-protection-from-Nexperia-combines-high-signal-integrity--low-clamping-voltage-and-high-surge-robustness/PR_image_TrEOS_Automotive_2100x1500px.png/jcr:content/PR_image_TrEOS_Automotive_2100x1500px.png)
Nexperia, the expert in essential semiconductors, has introduced four new TrEOS ESD protection devices that are AEC-Q101- qualified for automotive use and high temperature capable up to 175°C. In common with all TrEOS components, the new parts combine extremely low capacitance ensuring high signal integrity, extremely low clamping and high robustness for modern automotive interfaces. Specific automotive applications include infotainment, multimedia and ADAS systems featuring USB 3.2, HDMI, LVDS, SerDes and SD-card interfaces.
Nexperia’s TrEOS ESD protection technology uses active silicon-controlled rectification to overcome the traditional protection trade-off challenge. Capacitance is kept down to 0.5 pF, clamping voltage is just 3 V and devices can withstand surge and ESD pulses up to 10 A 8/20 µs. This industry-leading performance in all areas is delivered in the extensively-proven SOT23 package
Lukas Droemer, Nexperia product manager commented: “Our TrEOS technology has set the industry benchmark for mobile and computing ESD protection since its launch in 2015. Now, as there is a demand for more and more connectivity in vehicles, Nexperia is continuing to qualify its TrEOS ESD protection portfolio for the automotive sector. With these new parts, automotive design engineers can empower their new systems with the efficiency of TrEOS ESD protection while improving system-level robustness."
The first four PESD2USBx-T series AEC-Q101-qualified TrEOS ESD protection devices are in mass production now. More information including product specs and datasheets is available at www.nexperia.com/automotive-infotainment-serdes
About Nexperia
Nexperia is a leading expert in the high-volume production of essential semiconductors, components that are required by every electronic design in the world. The company’s extensive portfolio includes diodes, bipolar transistors, ESD protection devices, MOSFETs, GaN FETs and analog & logic ICs. Headquartered in Nijmegen, the Netherlands, Nexperia annually ships more than 90 billion products, meeting the stringent standards set by the automotive industry. These products are recognized as benchmarks in efficiency – in process, size, power and performance — with industry-leading small packages that save valuable energy and space.
With decades of experience in supplying to the world’s leading companies, Nexperia has over 12,000 employees across Asia, Europe and the US. Nexperia, a subsidiary of Wingtech Technology Co., Ltd. (600745.SS), has an extensive IP portfolio and is certified to IATF 16949, ISO 9001, ISO 14001 and OHSAS 18001.
Nexperia: Efficiency wins.
For press information, please contact:
Nexperia | Agency: BWW Communications |
Petra Beekmans, Head of Communications & Branding |
Nick Foot, director |