Nexperia announces new ESD protection devices for high-speed interfaces in automotive applications

Nexperia announces new ESD protection devices for high-speed interfaces in automotive applications

April 20, 2021

Nijmegen -- High performance 4-channel ESD protection for automotive multimedia and video link applications offering ideal signal integrity

Nexperia, the expert in essential semiconductors, has announced a new range of ESD protection devices aimed specifically at protecting the ever-increasing number of high-speed interfaces found in automotive applications, especially the in-vehicle networks (IVN) associated with infotainment and vehicle communications.

As data rates increase and vehicles feature more electric content, the need for EMC protection becomes more critical and providing the correct type of protection is a challenge for design engineers. Nexperia’s TrEOS technology optimizes the three pillars of ESD protection (Signal Integrity, System Protection and Robustness) to deliver devices with the ideal combination of low capacitance, low clamping voltage and high ESD robustness.

The new PESD4USBx series comprises a total of twelve high-performance 4-channel ESD protection devices that incorporate TrEOS technology. Signal integrity is ensured by the very low line capacitance for each channel (as low as 0.25 pF) and the sub-0.05 pF line matching capacitance. All devices offer deep snapback combined with a low resistance of 0.4 Ohm. With ESD protection up to ±15 kV, the PESD4USBx series meets IEC61000-4-2 level 4 and ISO10605. This is the highest level of ESD protection currently available in this package size making the devices ideal for modern, densely-packed, automotive designs.

A wide range of interface standards are supported including USB 2.0, Superspeed USB at 10 Gbps, HDMI 2.0, HDBaseT and the increasing number of automotive A/V monitors displays and cameras found in vehicles. PESD4USBx devices also support video links (SerDes): GMSL, FPD-Link and LVDS.

Specifically engineered for automotive applications, the devices exceed the needs of AEC-Q101 by a factor of two. Furthermore, in Nexperia’s state-of-the-art DFN2510D packages (SOT1165D and SOT1176D), side-wettable flanks (SWF) are available as standard, allowing the use of automatic optical inspection (AOI), thereby enhancing assembly quality for customers.

Commenting on the product launch, Lukas Droemer, Nexperia product manager said: “The electronic content is growing rapidly throughout the vehicle and, coupling this with the need for high data rates, interfaces commonly found in high-end A/V applications are becoming prevalent. With the heavy electrical content, vehicles are electrically noisy environments and these sensitive interfaces need high-performance ESD protection. Our new PESD4USBx series combines strong TrEOS performance with automotive grade quality specifically for demanding automotive multimedia applications.”

The new devices are available as samples and in production quantities today.

For more information visit Automotive infotainment/SerDes | Nexperia

 

About Nexperia

Nexperia is a leading expert in the high-volume production of essential semiconductors, components that are required by every electronic design in the world. The company’s extensive portfolio includes diodes, bipolar transistors, ESD protection devices, MOSFETs, GaN FETs and analog & logic ICs. Headquartered in Nijmegen, the Netherlands, Nexperia annually ships more than 90 billion products, meeting the stringent standards set by the automotive industry. These products are recognized as benchmarks in efficiency – in process, size, power and performance — with industry-leading small packages that save valuable energy and space.

With decades of experience in supplying to the world’s leading companies, Nexperia has over 12,000 employees across Asia, Europe and the US. Nexperia, a subsidiary of Wingtech Technology Co., Ltd. (600745.SS), has an extensive IP portfolio and is certified to IATF 16949, ISO 9001, ISO 14001 and OHSAS 18001.

Nexperia: Efficiency wins.

For press information, please contact:

Nexperia Agency: BWW Communications

Petra Beekmans, Head of Communications & Branding
Phone: +31 6 137 111 41
Email: petra.beekmans@nexperia.com

Nick Foot, director
Phone: +44-1491-636393
Email: Nick.foot@bwwcomms.com