Nexperia establishes new Application Specific FET category to deliver optimized performance
October 21, 2020Nijmegen -- ‘ASFETs’ feature MOSFET parameters tailored for particular applications

Nexperia, the expert in essential semiconductors, has responded to industry’s demands to maximize performance by defining a new MOSFET product group. Application Specific FETs (ASFETs) feature MOSFETs with optimized parameters for specific applications. By focusing on individual applications, significant improvements can be offered.
Nexperia is offering ASFET families for battery isolation, motor control, hot-swap and Power over Ethernet (PoE) applications. Defining the improvements that these tailored ASFETs can offer is application specific, examples include, 3x – 5x improvement in Safe Operating Area (SOA) for hot-swap applications, and maximum current ratings in excess of 300 A for motor applications.
Commented Chris Boyce, Senior Director for the Power MOSFETs Group at Nexperia: “As designers push the boundaries of performance, it is crucial to understand how the MOSFET will be used in the application. There are 100+ parameters on a regular MOSFET datasheet but usually only a few are critical in each project. However, as the applications change, so do the critical parameters. At Nexperia, we determine the performance of every element of our products; the core silicon technology, the chip design, the package and the manufacturing & test procedures. By keeping individual application requirements front & centre of our thinking, we can choose to optimise the parameters that matter most in a particular use-case, often at the expense of others of less relevance. In essence we have combined our proven MOSFET expertise with a broad understanding of applications so we can tailor products which offer the ultimate performance for a specific application or functionality.”
The ASFET category will be further enhanced with the imminent release of a new family of automotive products with guaranteed repetitive avalanche performance for driving inductive loads.
Added Boyce: “We are continually seeking to deepen our understanding of specific applications, often working hand-in-hand with our customers. In exposing our best engineers to detailed application requirements, we are opening new and exciting possibilities of innovation – there are many more ASFET advances in the pipeline.”
More details are available at: https://efficiencywins.nexperia.com/efficient-products/optimizing-mosfets-to-fit-specific-applications.html
About Nexperia
Nexperia is a leading expert in the high-volume production of essential semiconductors, components that are required by every electronic design in the world. The company’s extensive portfolio includes diodes, bipolar transistors, ESD protection devices, MOSFETs, GaN FETs and analog & logic ICs. Headquartered in Nijmegen, the Netherlands, Nexperia annually ships more than 90 billion products, meeting the stringent standards set by the automotive industry. These products are recognized as benchmarks in efficiency – in process, size, power and performance — with industry-leading small packages that save valuable energy and space.
With decades of experience in supplying to the world’s leading companies, Nexperia has over 12,000 employees across Asia, Europe and the US. Nexperia, a subsidiary of Wingtech Technology Co., Ltd. (600745.SS), has an extensive IP portfolio and is certified to IATF 16949, ISO 9001, ISO 14001 and OHSAS 18001.
Nexperia: Efficiency wins.
For press information, please contact:
Nexperia | Agency: BWW Communications |
Petra Beekmans, Head of Communications & Branding |
Nick Foot, director |