Nexperia expands logic portfolio with new voltage translator devices
December 18, 2017Nijmegen -- Low-power translator solution now addresses standard logic shift register market

Nexperia, the former Standard Products division of NXP, today announced that it is expanding its logic portfolio – already the largest in the industry – with new devices that expand the company‘s translator solutions into the standard logic shift register arena.
The first translator solution in the expanded range, 74LVC8T595 is a world’s first: a cascadable 8-bit serial-in, parallel-out I/O expansion device that combines shift register function with voltage translation. This single-chip solution replaces two devices, delivering higher levels of integration and a smaller footprint. It operates in the 1.1 to 5.5 V range, enabling newer low-voltage controllers to interface with legacy solutions.
74LVC8T595 benefits from Nexperia’s LVC family technology with IOFF circuitry for partial power down-mode operation, which contributes to energy savings. The device is available in 20-pin leaded TSSOP and leadless DQFN packages. Both packages are specified for -40 °C to +125 °C and can be released in the company’s Automotive (-Q100) portfolio.
Nexperia already markets the lowest power 5V, 3.3V and 1.8.V translator solutions and it is bringing this capability to its new standard logic voltage translating shift register products. Commented Nexperia’s Senior Product Manager for Logic, Michael Lyons: “These new devices are helping to create a market by enabling voltage-level translation for new low-voltage controllers to interface with legacy solutions and vice versa. Our devices save space and BOM costs and help to improve system integration and performance.“
About Nexperia
Nexperia, the former Standard Products division of NXP, is a dedicated global leader in Discretes, Logic and MOSFETs devices. The company became independent at the beginning of 2017. Focused on efficiency, Nexperia produces consistently reliable semiconductor components at high volume: 85 billion annually. Our extensive portfolio meets the stringent standards set by the Automotive industry. Industry-leading, miniature packages, produced in our own manufacturing facilities, combine power and thermal efficiency with best-in-class quality levels.
With over 50 years history supplying to the world’s biggest companies, Nexperia has 11,000 employees across Asia, Europe and the U.S., offering global support. The company has an extensive IP portfolio and is certified to ISO9001, ISO/TS16949, ISO14001 and OHSAS18001.
Nexperia: Efficiency wins.
For press information, please contact:
Nexperia | Agency: BWW Communications |
Petra Beekmans, Head of Communications & Branding |
Nick Foot, director |