Nexperia introduces new generation of high performance In-Vehicle Network protection diodes
December 14, 2017Nijmegen -- Drop-in replacements have higher surge current, greater ESD robustness and much better ESD clamping.
Nexperia, the former Standard Products division of NXP, today announced a new generation of in-vehicle network (IVN) protection diodes that offer a higher surge current, greater ESD robustness and a significant improvement in ESD clamping performance. The new AEC-Q101 qualified PESDxIVN series of surface mount devices is optimized for the latest generation of CAN, LIN, and FlexRay transceivers.
The new parts are drop-in replacement for legacy devices, available in familiar SOT23, SOD323 and SOT323 packages. However the new parts deliver higher performance. For example, PESD2IVN24-T parts deliver a 30 kV ESD robustness (up from 23 kV on the legacy PESD1CAN), an improved surge current of 3.5 A and much better clamping of 42 V at 3.5 A (was 70 V at 3 A). Other parameters remain constant or slightly better. The PESD1IVN27-A offers the same improvement in ESD robustness with a lower (=better) clamping voltage compared to the legacy PESD1LIN.
Commented Nexperia’s Marketing Manager Automotive André Dressler: “In modern vehicles there is an increasing amount of data exchange and the electronic content is growing in functionality and complexity, therefore effective ESD protection solutions are imperative. Nexperia has brought on-line a massive capacity increase for ESD diodes in order to guarantee a secure chain, and provide customers with peace of mind that they are protecting the electronics in their vehicles with high-performance, rugged and efficient devices.”
For press information, please contact:
Nexperia | Agency: BWW Communications |
Petra Beekmans, Head of Communications & Branding |
Nick Foot, director |
About Nexperia
Nexperia, the former Standard Products division of NXP, is a dedicated global leader in Discretes, Logic and MOSFETs devices. The company became independent at the beginning of 2017. Focused on efficiency, Nexperia produces consistently reliable semiconductor components at high volume: 85 billion annually. Our extensive portfolio meets the stringent standards set by the Automotive industry. Industry-leading, miniature packages, produced in our own manufacturing facilities, combine power and thermal efficiency with best-in-class quality levels.
With over 50 years history supplying to the world’s biggest companies, Nexperia has 11,000 employees across Asia, Europe and the U.S., offering global support. The company has an extensive IP portfolio and is certified to ISO9001, ISO/TS16949, ISO14001 and OHSAS18001.