Nexperia launches industry-first LED drivers in DFN package with side-wettable flanks
October 12, 2020Nijmegen -- AEC-Q101-qualified DFN2020D-6 devices save up to 90% PCB space; side-wettable flanks enable automated inspection (AOI) and improve reliability
![](/.imaging/mte/nexperia/page-intro/dam/nexperia/About-new_final/News-and-Events/Press-release/press-releases/Nexperia-launches-industry-first-LED-drivers-in-DFN-package-with-side-wettable-flanks/Nexperia-Press-image-LED-Driver.jpg/jcr:content/Nexperia%20Press%20image%20LED%20Driver.jpg)
Nexperia, the expert in essential semiconductors, today announced a new range of LED drivers in the space-saving DFN2020D-6 (SOT1118D) package. This case style features side-wettable flanks (SWF) which facilitate the use of AOI (automated optical inspection), and improve reliability. This is the first time LED drivers have been available in this beneficial package. The new leadless devices join Nexperia’s wide range of LED drivers in leaded packages offering equivalent performance yet reducing PCB space by up to 90% compared to SOT223.
With a footprint of just 2x2 mm and a low profile of 0.65 mm, the new DFN2020D-6 LED drivers are available in NPN technology. They feature an output current of up to 250 mA (NCR32x types) and a maximum supply voltage of 40 V. Their high thermal power capability is at least equal to any other package for LED drivers.
The use of side-wettable flanks not only enables AOI techniques to be used - which is especially important for automotive customers – but also improves reliability. Devices with side-wettable flanks exhibit a greater resistance to shear forces, and can handle greater board flexing without cracking than devices without side-wettable flanks.
Commented Frank Matschullat, product group manager at Nexperia: “The new DFN2020D-packaged parts with SWF address the concerns of various sectors – size, performance, ruggedness – so they are a perfect match for many diverse applications in general lighting, white goods and automotive. Nexperia is committed to deliver industry’s broadest discrete portfolio in DFN technology, so introducing LED drivers in this rugged, space-saving package is a natural step. However, parts are also available in leaded SMD styles so customers can choose which to use.”
Four DFN2020D-6 LED drivers are in mass production now. More information including product specs and datasheets is available at www.nexperia.com/led-driver.
About Nexperia
Nexperia is a leading expert in the high-volume production of essential semiconductors, components that are required by every electronic design in the world. The company’s extensive portfolio includes diodes, bipolar transistors, ESD protection devices, MOSFETs, GaN FETs and analog & logic ICs. Headquartered in Nijmegen, the Netherlands, Nexperia annually ships more than 90 billion products, meeting the stringent standards set by the automotive industry. These products are recognized as benchmarks in efficiency – in process, size, power and performance — with industry-leading small packages that save valuable energy and space.
With decades of experience in supplying to the world’s leading companies, Nexperia has over 12,000 employees across Asia, Europe and the US. Nexperia, a subsidiary of Wingtech Technology Co., Ltd. (600745.SS), has an extensive IP portfolio and is certified to IATF 16949, ISO 9001, ISO 14001 and OHSAS 18001.
Nexperia: Efficiency wins.
For press information, please contact:
Nexperia | Agency: BWW Communications |
Petra Beekmans, Head of Communications & Branding |
Nick Foot, director |