Nexperia introduces new high speed optimized flip-chip package technology for automotive ESD protection

Nexperia introduces new high speed optimized flip-chip package technology for automotive ESD protection

April 09, 2025

Nijmegen -- New flip-chip land grid array (FC-LGA) packages deliver superior RF performance and meet
automotive quality with industry's first side-wettable flank versions

Nexperia today announced a new portfolio of high signal integrity, bidirectional electrostatic discharge (ESD) protection diodes in innovative flip-chip land-grid-array (FC-LGA) packaging. This new package technology is optimized for protecting and filtering high-speed data communication links which are increasingly used in modern cars. Applications like in-vehicle camera video-links, multi-gigabit automotive Ethernet networks as well as infotainment interfaces like USBx, HDMIx, and PCIex, can be protected against potentially damaging ESD events.

Flip-chip packages have minimal parasitic components – they come without bond wires or copper lead frames resulting in high performance and excellent signal integrity. Nexperia’s new 2- and 3-pin FC-LGA diodes have ultra-low capacitance (<0.25 pF) and insertion loss (-3 dB at 14.6 GHz) – features that are key for use in high data rate applications. Both flip-chip packages, the 2-pin DFN1006L(D)-2 and the 3-pin DFN1006L(D)-3, share the same footprint as their standard counterparts, ensuring drop-in compatibility. They offer up to 6 GHz bandwidth improvement compared to conventional DFN technologies. Moreover, the 3-pin devices’ ability to protect two channels and offer capacitance matching saves more space while further improving circuit performance and stability.

Apart from offering best-in-class signal integrity, this family of diodes also comes with the industry’s widest range of reverse working voltages (Vrwm), including 5 V, 18 V, 24 V and 30 V options. Higher voltage devices provide the additional advantage of flexible board placement for protecting multiple devices connected at various points along a link. With products like the PESD5V0H1BLG-Q in DFN1006LD-2 and PESD5V0H2BFG-Q in DFN1006LD-3 packaging Nexperia is the only supplier to offer ESD protection diodes in flip-chip packaging with side-wettable flanks (SWF). This enables the use of automated optical inspection (AOI) of solder joints to ensure that they meet the exacting quality requirements of the automotive industry, where safety is paramount.

"These new diodes combine side-wettable flanks with a DFN1006 footprint optimized for maximum signal integrity and represent a significant improvement to the options currently available. Designed to support the growing trend of data-intensive automotive applications, they reflect Nexperia's proven expertise in packaging technology. This launch reinforces our commitment to delivering innovative solutions that meet the evolving demands of engineers across a wide range of industries," says Alexander Benedix, Head of Product Group Protection and Filtering at Nexperia.

The first three 5 V Flip-Chip diodes are in mass production. Six products with 18 V, 24 V and 30 V are sampling and will be available in mass production in Q2 2025. To learn more about Nexperia’s ESD protection diodes in FC-LGA visit: High speed automotive ESD

About Nexperia

Headquartered in the Netherlands, Nexperia is a global semiconductor company with a rich European history and over 12,500 employees across Europe, Asia, and the United States. As a leading expert in the development and production of essential semiconductors, Nexperia’s components enable the basic functionality of virtually every commercial electronic design in the world – from automotive and industrial to mobile and consumer applications.
The company serves a global customer base, shipping more than 100 billion products annually. These products are recognized as benchmarks in efficiency – in process, size, power, and performance. Nexperia's commitment to innovation, efficiency, sustainability, and stringent industry requirements is evident in its extensive IP portfolio, its expanding product range, and its certification to IATF 16949, ISO 9001, ISO 14001 and ISO 45001 standards.

For press information, please contact:

Nexperia
Anne Proch
Tel: +49 160 916 884 18
Email: anne.proch@nexperia.com

Publitek
Lucy Sorton
Tel: +44 07966 301949
E-mail: lucy.sorton@publitek.com