Nexperia launches new portfolio of application specific MOSFETs (ASFETs) for automotive airbags
May 12, 2022Nijmegen -- Provides excellent transient linear mode performance using new SOA trench technology in LFPAK packaging providing designers with a smaller and more reliable choice.

Nexperia, the expert in essential semiconductors, has launched a new portfolio of application specific MOSFETs (ASFETs) for automobile airbag applications, headlining with the release of the BUK9M20-60EL single N-channel 60 V, 13 mOhm logic level MOSFET in LFPAK33 packaging. ASFETs are MOSFETs that have been specifically designed and optimized for use in one application. This portfolio is the latest addition to a range of other ASFETs which Nexperia’s provides for battery isolation, motor control, hot-swap, and Power-over-Ethernet (PoE) applications.
The BUK9M20-60EL uses Nexperia’s new enhanced safe operating area (SOA) technology which has been tailored to provide exceptional transient linear mode performance, a key performance metric in airbag applications. The BUK9M20-60EL achieves this performance in new LFPAK33 packaging which uses 84% less board space when compared to older DPAK packaging, while still maintaining robustness.
“Other similar products use older DPAK packaging and are typically based on DMOS and first-generation trench technologies which are being gradually retired by many silicon manufacturers,” according to Norman Stapelberg, Senior Product Marketing Manager at Nexperia. “This portfolio of ASFETs uses a combination of the latest silicon trench technology and LFPAK packaging, allowing it to meet the most recent reliability standards. Using the latest manufacturing and packaging technologies makes the supply chain more sustainable and empowers Nexperia to increase capacity to meet the demands of a growing market for these products.”
For more details on the BUK9M20-60EL visit: https://www.nexperia.com/products/mosfets/automotive-mosfets/BUK9M20-60EL.html
For more details on Nexperia’s ASFETs visit:
About Nexperia
Nexperia is a leading expert in the high-volume production of essential semiconductors, components that are required by every electronic design in the world. The company’s extensive portfolio includes diodes, bipolar transistors, ESD protection devices, MOSFETs, GaN FETs and analog & logic ICs. Headquartered in Nijmegen, the Netherlands, Nexperia annually ships more than 100 billion products, meeting the stringent standards set by the automotive industry. These products are recognized as benchmarks in efficiency – in process, size, power, and performance — with industry-leading small packages that save valuable energy and space.
With decades of experience in supplying to the world’s leading companies, Nexperia has over 14,000 employees across Asia, Europe, and the US. Nexperia, a subsidiary of Wingtech Technology Co., Ltd. (600745.SS), has an extensive IP portfolio and is certified to IATF 16949, ISO 9001, ISO 14001, and ISO 45001.
Nexperia: Efficiency wins.
For press information, please contact:
Nexperia
Petra Beekmans, Head of Communications & Branding
Phone: +31 6 137 111 41
Email: petra.beekmans@nexperia.com