Advanced Electrothermal models from Nexperia cover entire MOSFET operating temperature range
March 24, 2022Nijmegen -- New models also enable investigation of EMC performance even before prototyping
![](/.imaging/mte/nexperia/page-intro/dam/nexperia/About-new_final/News-and-Events/Press-release/press-releases/Advanced-Electrothermal-models-from-Nexperia-cover-entire-MOSFET-operating-temperature-range/NEXP_017_PR-image_Electrothermal_Models.jpg/jcr:content/NEXP_017_PR%20image_Electrothermal_Models.jpg)
Nexperia, the expert in essential semiconductors, today announced the release of new, enhanced Electrothermal models for its MOSFET devices. Semiconductor manufacturers commonly provide simulation models for their MOSFETs, but these usually only include a limited number of device parameters which have been modelled at typical operating temperatures. Nexperia’s new advanced models capture the thermal interdependency of the complete set of device parameters right across the full operating temperature range from -55 °C to 175 °C.
Overall accuracy is further enhanced by the inclusion of reverse diode recovery time and device electromagnetic compatibility (EMC) performance in these advanced models. These enable engineers to create accurate circuit and system level simulations and assess the electrical, thermal and EMC performance before committing to build a prototype. These models also help save time and resources because engineers, who were previously required to ensure that their designs could operate under (unlikely) worst-case conditions, can now simulate their designs across specific temperatures ranges.
Nexperia developed these models in close partnership with a Tier 1 OEM whose requirements could not be satisfied by any others currently available. “These new advanced electrothermal models are intended to give designers the ultimate degree of confidence in the results of their circuit simulations” according to Andy Berry, applications engineer with Nexperia. “Their unprecedented level of precision is evidenced by how accurately the models predict real device behaviour during double pulse testing. Initial feedback from our collaborative partner indicates that these models are the most exact they have ever seen.”
Following on from the unveiling of Nexperia’s popular interactive application notes, these advanced electrothermal models are the latest in a series of next generation support tools, designed by engineers for engineers, planned for release over the coming months. This new approach to supporting external activity is intended to make device design-in as seamless as possible for Nexperia’s customers.
For more information visit www.nexperia.com/advanced-support-tools
About Nexperia
Nexperia is a leading expert in the high-volume production of essential semiconductors, components that are required by every electronic design in the world. The company’s extensive portfolio includes diodes, bipolar transistors, ESD protection devices, MOSFETs, GaN FETs and analog & logic ICs. Headquartered in Nijmegen, the Netherlands, Nexperia annually ships more than 100 billion products, meeting the stringent standards set by the automotive industry. These products are recognized as benchmarks in efficiency – in process, size, power and performance — with industry-leading small packages that save valuable energy and space.
With decades of experience in supplying to the world’s leading companies, Nexperia has over 12,000 employees across Asia, Europe and the US. Nexperia, a subsidiary of Wingtech Technology Co., Ltd. (600745.SS), has an extensive IP portfolio and is certified to IATF 16949, ISO 9001, ISO 14001 and ISO 45001.
Nexperia: Efficiency wins.
For press information, please contact:
Nexperia
Petra Beekmans, Head of Communications & Branding
Phone: +31 6 137 111 41
Email: petra.beekmans@nexperia.com
Judith Schröter
Phone: +49 170 8586403
Email: judith.schroeter@nexperia.com
Publitek
Björn Oberhössel
Phone: +49 4181 968098-30