Ultra-low capacitance ESD protection diodes from Nexperia protect automotive data interfaces

Ultra-low capacitance ESD protection diodes from Nexperia protect automotive data interfaces

August 01, 2022

Nijmegen -- Robust protection devices minimize their impact on signal integrity

Nexperia, the expert in essential semiconductors, today announced an extension to its portfolio of extremely low clamping and ultra-low capacitance ESD protection diodes. This portfolio is designed to protect high-speed data lines such as USB 3.2, HDMI 2.0, LVDS, automotive A/V Monitors, displays and cameras. Additionally, this portfolio also aims to address the upcoming high-speed video-links as well as the OPEN Alliance MGbit ethernet applications.

These latest product additions include PESD5V0C1BLS-Q and PESD5V0C1ULS-Q both as 2-pin single line devices with very compact DFN1006BD-2 package for optimized routing flexibility. In addition, PESD5V0C2UM and PESD5V0C2UM-Q are available as 3-pin devices for both differential lines in DFN1006-3. All variants come in leadless packages to improve electrical performance and signal integrity.

Electrostatic discharge (ESD) voltage clamping diodes perform a vital function by protecting data interfaces in automotive subsystems from damage. However, it is important that they do not degrade data signal integrity or negatively impact the electromagnetic compatibility (EMC) performance of the systems which they protect. Nexperia’s long-standing expertise in the design of ESD protection solutions has allowed these diodes to provide best-in-class signal integrity performance because of their ultra-low device capacitance (as low as 0.3 pF). For maximum design flexibility these diodes are offered in both dual line DFN1006-3 and single line DFN1006BD-2. With the latter packages having side wettable flanks to enable automated optical inspection (AOI).

These AEC-Q101 automotive qualified devices exhibit deep snapback behavior combined with a low resistance of 0.27 Ω, for improved system level robustness and clamping performance in high-speed data interfaces.

For device and datasheets more information visit: Nexperia.com/automotive-ESD-protection.

About Nexperia

Nexperia is a leading expert in the high-volume production of essential semiconductors, components that are required by every electronic design in the world. The company’s extensive portfolio includes diodes, bipolar transistors, ESD protection devices, MOSFETs, GaN FETs and analog & logic ICs. Headquartered in Nijmegen, the Netherlands, Nexperia annually ships more than 100 billion products, meeting the stringent standards set by the automotive industry. These products are recognized as benchmarks in efficiency – in process, size, power and performance — with industry-leading small packages that save valuable energy and space.

With decades of experience in supplying to the world’s leading companies, Nexperia has over 14,000 employees across Asia, Europe and the US. Nexperia, a subsidiary of Wingtech Technology Co., Ltd. (600745.SS), has an extensive IP portfolio and is certified to IATF 16949, ISO 9001, ISO 14001 and ISO 45001.

For press information, please contact:

Nexperia

Petra Beekmans, Head of Communications & Branding

Phone: +31 6 137 111 41

Email: petra.beekmans@nexperia.com

 

Judith Schröter

Phone: +49 170 8586403

Email: judith.schroeter@nexperia.com

 

Publitek

Natalia Selezneva

Phone: +49 4181 968098-16

Email: natalia.selezneva@publitek.com